7/10/2020 8:17 AM | |
Joined: 7/2/2020 Last visit: 2/28/2023 Posts: 14 Rating:
|
hello, i meant if there is a M code to put it in MDA to reset magazine to 0, i have no tools in magazine, no tools in preloader, so maybe there is a M code to tell the machine that everythink is empty. The problem is that i don t have any backup of nc data. Preloader loads corectly the tools with the coresponding pocket that i set, but somehow it always tryes to put the tools to location 0002, even if i disable that location, so if i do N20 T=''T5'', N30 M6, then the magazine roates to pocket 5, the POT goes down and this is it, the error says that tool T5 cannot be putet on location 0002, invalid definition of magazine. It doesn't have sense, from my opinion. When the error come L13 led is flashing in electrical panel, i put a small video of that. Anyway i dont think i will solve this.
Attachmentvideo-1594361258.avi (487 Downloads) |
Follow us on