10/18/2021 9:54 AM | |
Posts: 5 Rating: (0) |
Hello expert I have same error A831 and checked profibus and its connected good but still same error . So could help me to trace this error . send the model of simodrive 611
------------------------------------------------------------------------------------------ |
Last edited by: Mohammed92 at: 10/18/2021 09:59:59Last edited by: Jen_Moderator at: 10/18/2021 12:59:28New subject after splitting |
|
10/19/2021 5:43 AM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Hello, I guess this is the same problem discussed under Simo drive 611 e 831 topic. 1. Have you checked all profibus connectors? Even if failuer of single connector or cable connection interupts communication & trigers 831 fault. 2. If profibus cable (complete), all connectors are OK, then try by replacing control card. |
This contribution was helpful to1 thankful Users |
10/19/2021 5:52 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Simo drive 611 e 831 is published within the conference SIMODRIVE Converter system. Best regards, |
This contribution was helpful to1 thankful Users |
Follow us on