8/9/2018 11:11 AM | |
Joined: 10/15/2014 Last visit: 7/13/2023 Posts: 5 Rating: (0) |
Hello, I have strange problem at Weiler E35 lathe with Sinumerik CPU810DE CCU1 SW version 1.6. To make long story short, the HDD died completely, no image of disk, so I find another Weiler E35 lathe, clone a disk and put it into MMC panel. Since the HDD was of a slightly newer Weiler, many of the operator functions keys was not working, so have to instal the user interface program of the newer lathe via menu, accessible with number 6 at startup. All keys responsive now, NC and PLC backup reloaded, machine operational, can reference axis, turn the spindle and so on. The problem arise, when I try to enter the value at the spindle constant turning speed, machine return error at DDI access. This seems a typo in the error list file, I think that must be error at DDE access the corect statement. The same error occur, when trying to enter new tool or make new cycle or program.Same error in simulation also. I think, that the problem may be in the file mmc.ini, or is this completely wrong? Thank you all for suggestions. AttachmentPics.zip (74 Downloads) |
Follow us on