10/4/2010 2:54 PM | |
Joined: 4/9/2010 Last visit: 5/23/2024 Posts: 222 Rating: (33) |
Hello, I have the same error code on startup ofWinCC Flexible Runtime 2008 SP2 Upd. 3 when trying to connect to S7-226 rel 02.01. The connection parameters are shown in the enclosed screen snapshots. Help file says I shouldn't use the USB PPI cable but apparently it does work for other users. I hope trying RS232 PPI cable today but any help using USB cable I have would be greatly appreciated. Regards, Adam Splitted from error code 0x80000104. Attachment0x80000104.pdf (602 Downloads) |
Last edited by: O_Moderator at: 10/5/2010 9:05 AMLast edited by: O_Moderator at: 10/5/2010 9:05 AMnew subject after splitting Last edited by: adam_ski at: 10/4/2010 2:56 PM |
|
Follow us on