9/3/2017 4:44 PM | |
Posts: 2 Rating: (0) |
Hi Ash, I have a same error code 1739:60458 but c_prtbas. I dont know what is the meaning of this error code. But this happen when im creating activation code for CPU410-5H AS RT PO. is your solution applicable for these? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/12/2017 3:20:31 PMNew subject after splitting |
|
9/27/2017 8:14 AM | |
Joined: 4/8/2016 Last visit: 10/1/2024 Posts: 133 Rating: (45) |
Hello, I found a note in a FAQ, which might be helpful: "In some cases you can receive the following error when downloading changes while RUN: This error is caused by exceeding the maximum amount of PBC blocks while downloading changes. Here is the link: https://support.industry.siemens.com/cs/ww/en/view/2446042 |
Last edited by: 51N3P at: 9/27/2017 8:14:49 AMKind regards |
|
9/11/2020 12:20 AM | |
Joined: 1/21/2013 Last visit: 3/20/2024 Posts: 24 Rating: (8) |
I had a problem to download or to access the AS. I needed to correct 2 things: After those corrections we had no errors anymore. PCS7 V8.0 SP1 |
Follow us on