11/10/2017 11:15 AM | |
Joined: 3/2/2007 Last visit: 4/26/2024 Posts: 929 Rating: (5) |
Kindly, we have the below masterdrive with T300 board. It is damaged. So we tried to replace it by the second drive below, by removing the CUVC CBP2 T300 boards from the first, and installing them in the second. But we got an error “ E “ on the second drive display. What does this error “ E “ mean? 6SE7023-4TC61-Z G93+K01+K11, SIMOVERT MASTERDRIVESVECTOR CONTROL INVERTER COMPACT UNIT, IP20 510-650V DC, 34 A NOM. POWER RATINGS:15KWDOCUMENTATION ON CD ***SPARE PART*** G93=COMMUNICATIONS MODULE PROFIBUS CBP2, SLOT C ***SPARE PART*** K01=ADAPTER MODULE FOR SLOT D AND E , K11=LOCAL BUS ADAPTER FOR ELECTRONIC BOX LBA 6SE7024-7TD61-Z G91, SIMOVERT MASTERDRIVESVECTOR CONTROL INVERTER COMPACT UNIT, IP20 510-650V DC, 47 A NOM. POWER RATINGS:22KWDOCUMENTATION ON CD , G91=COMMUNICATIONS MODULE PROFIBUS CBP2, SLOT A |
... thank you ... |
|
Follow us on