12/10/2020 4:41 AM | |
Posts: 17 Rating: (0) |
Hi guys, I am facing the same issue. Error message: Module exists. Error Error in lower-level component Additional information for the module: Differences were found between the loaded configuration and the offline project. Online article number: 6SL3 040-1MA01-0AA0 Offline article number: 6SL3 040-1MA01-0AAx I just couldn't understand why does the last unit "0" vs "x" can caused me this error. So I am using S7-1211C ver4.2 with Sinamics S120-CU320-2-PN ver4.8 I had downloaded and installed the latest Profinet-IO gsd file (gsd v2.34 s120-cu3x) I had tried extended download, hardware download only, software download only but nothing seems to be working. Any suggestions? Much help will be appreciated. Thanks AttachmentError Lower-Level Component.zip (659 Downloads) |
Follow us on