11/15/2023 7:11 AM | |
Joined: 8/13/2020 Last visit: 5/9/2024 Posts: 19 Rating: (0) |
Hello everyone, Machine details DMG NEF600 SINUMERIK 840D NCU 571.5 - 6FC5357-0BB15-0AA0 I am facing a problem in one machine with Sinumerik 840D NCU, initially in the HMI it was showing "Waiting for NCK connection". In the NCU , digit 6 was there, POK- green PR- light OFF, PS- red, PF- Red. Then I make a memory reset and I downloaded the backups. After that POK and PR are showing green, PS and PF are OFF. But when operator try to enable Shop turn, in the loading screen its showing a message" Error in MC_AXCONF_MACHAX_USED: Entry missing". What could be the reason for this error?? When the operator try to operate the machine in manual mode, getting an alarm as "17040: Channel 1 block-illegal axis index". In auto mode the alarm is "16100 Channel 1 block 2 spindle as not available in the channel". Another alarm is "12560: Channel 1 block programmed value S65535= exceeds allowed limits". For alarm 16100, as per the diagnostic manual the parameters MD35000 and MD20070 are verified with working machine and found to be same. Kindly suggest how to troubleshoot this. Photos are attached. Thanks in advance AttachmentAlarms.zip (225 Downloads) |
Follow us on