8/18/2016 6:29 AM | |
Posts: 5 Rating: (0) |
Hi. Can no one help my by this Problem? |
4/6/2018 9:59 AM | |
Posts: 7 Rating: (0) |
Dear Expert Dear all Kindly advice is there change made on new version iIP627C6EQ2020-0AC03-5XX0 which limits Simatic BoxPC 627B 6EQ2020-0AB12-5XX0 programmes to work with it This information could it be found on CD for the new version. The main challenge on the ground is as per below in Bold type & Underlined. Kindly advise how we can tackle it or we have to get the CD for the new version ie IP627C6EQ2020-0AC03-5XX0.Please assist ASAP The question is how do we load the PC name and IP address? Dear Sir/Madam The attached file clientaccesstable.txt is to be copied to the IEM. But when copied it does not save some information which is vital for the PC to accesses the IEM. The information lacking is as below. You can compare the two files and see at the bottom of each file. # Add your entries to the Client Access Table below: 192.168.100.125 ACFCENGG 192.168.101.135 ACFCENGG 192.168.100.101 ACFCSERV1 192.168.101.111 ACFCSERV1 192.168.100.102 ACFCSERV2 192.168.101.112 ACFCSERV2 192.168.100.110 ACFCLAP Attachmentclientaccesstable.txt (100 Downloads) |
4/6/2018 10:00 AM | |
Posts: 7 Rating: (0) |
Dear Expert Dear all Kindly advice is there change made on new version iIP627C6EQ2020-0AC03-5XX0 which limits Simatic BoxPC 627B 6EQ2020-0AB12-5XX0 programmes to work with it This information could it be found on CD for the new version. The main challenge on the ground is as per below in Bold type & Underlined. Kindly advise how we can tackle it or we have to get the CD for the new version ie IP627C6EQ2020-0AC03-5XX0.Please assist ASAP The question is how do we load the PC name and IP address? Dear Sir/Madam The attached file clientaccesstable.txt is to be copied to the IEM. But when copied it does not save some information which is vital for the PC to accesses the IEM. The information lacking is as below. You can compare the two files and see at the bottom of each file. # Add your entries to the Client Access Table below: 192.168.100.125 ACFCENGG 192.168.101.135 ACFCENGG 192.168.100.101 ACFCSERV1 192.168.101.111 ACFCSERV1 192.168.100.102 ACFCSERV2 192.168.101.112 ACFCSERV2 192.168.100.110 ACFCLAP WE HAVE NEW VERSION THE CHALLENGES IS PER ABOVE Attachmentoldclientaccesstable (1).txt (107 Downloads) |
4/6/2018 10:54 AM | |
Posts: 7 Rating: (0) |
Kindly update anyone to help will appreciate |
Follow us on