10/23/2007 1:30 PM | |
Posts: 947 Rating: (45) |
Hi! I use Step7 5.4SP2. I make project - see attachement (sgp.zip). In adress overiew HW- condig for CPU414-2 i see adress 2 for node 3 (PM-E), Project not use adress 6, I can't set adress PM-E 6 in node 5 - it's used. I delete node 5, adress 6 - not deleted: see adress overiew in screenshot (sgp2.gif); I delete node 3, adress 2 - not deleted: see adress overiew screenshot (sgp3.gif). After delete nodes 3 or 5 i can't compile HW-config. I receive message on error.
I make export from HW-config in file and import this file in Hw-config. After import i See error in config. All this is error in step7?. How i can delete node 5 without make new HW-condig? AttachmentSGP.zip (217 Downloads) |
10/23/2007 3:51 PM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, Maybe SP3 solves your problem. Sp3 is downloadable via this link. |
Smurf |
|
Follow us on