1/23/2018 12:36 PM | |
Joined: 4/29/2016 Last visit: 9/16/2024 Posts: 31 Rating: (1) |
Hello, I am facing the same error on WinCC Explorer v7.4. Runtime is running successfully and communicating with S7-400H PLC. suddenly, this error message is coming and a system is going to log off. With that error message one another message is coming, also. it is as follows "system is running on memory low". Now, we need to restart our pc and start wincc. for some time it is working fine and after that , further this error message is coming and the system is loged off. needs solution for that, I cannot understand what is occurring in the system, Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 23.01.2018 13:52:13Neue Überschrift nach Splitten |
|
Follow us on