Industry Online Support
Technical Forum
3/28/2014 10:14 AM | |
Posts: 1368 Rating:
|
Hello, you can use the Organisation blocks like OB82/83. This OB are called, if an error occurs e.g. a module fails. Here, you can react, build an own message or set a variable and show these for example withthe user defined webpage of the plc. Or you use the FB126; only the database with all the information of the error/faulty module. These information you also can show on a user defined webpages, if you have no WinCC. Edit: Perhaps here you also find some ideas: http://support.automation.siemens.com/WW/view/de/24000238 Greetings... |
Last edited by: Pittiplatsch at: 3/28/2014 10:27 AM |
|
Follow us on