6/23/2021 9:13 AM | |
Posts: 2 Rating:
|
Hai All I have 2 Wincc with redundant server and 1 Wincc Client with the same problem ( WINCC v7.4+SP1 Upd 11 ) Where The Client Runtime Error "No Start Screen", I have configured the Client File See photo attachment below Please help me to be able to solve this problem ------------------------------------------------------------------------------------------ AttachmentClient Configuration.zip (111 Downloads) |
Last edited by: Jen_Moderator at: 06/23/2021 12:45:31New subject after splitting |
|
6/23/2021 1:51 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello Irwin.S41, with which Windows-User you are logged in on Server see FAQ: https://support.industry.siemens.com/cs/ww/en/view/868014 3. Operating system The simplest way is, to have the same user and password on Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
6/25/2021 4:18 AM | |
Posts: 2 Rating:
|
Hai Dear Currently I am using the Windows 10 operating system, and in this case I have configured Folder Sharing both on the Server and on the Client and everything has been read on the network and turned off Password protection for the sharing folder. Here's the IP address I'm currently using 1. Scada 1 Server ( 192.168.0.10 ) 2. Scada 2 Backup Server ( 192.168.0.11 ) 3. Scada Client ( 192.168.0.7 ) But when I try to upload the .pck file back from the Server ( Scada-1) this problem still occurs. Scada Client cannot bring up the Start Screen where I see a description on Wincc Explore in "ACTIVE" condition. Note: Based on the information I received where the Operator tried to reboot the Client PC but I don't know they did it procedurally or did a hard restart of the PC Thank's AttachmentScada Client.zip (109 Downloads) |
Follow us on