12/9/2022 10:33 AM | |
Joined: 5/17/2018 Last visit: 1/26/2024 Posts: 2 Rating: (0) |
Hello, after installation of Tia Portal V17 Update 5 i have this problem when I try to compile a project that use wincc runtime advanced panel with some script inside it. The error detail is output directly after compiling the vb script The message error is "Due to a missing system component, the VB Script check failed. Please contact SIEMENS customer service." This problem don't occur when i try to compile the same script into a comfort panel. Has anyone already had this problem? I have attached the file with the export of the software currently installed on my pc. Attachmentinstalled_software_tiaV17.txt (205 Downloads) |
Follow us on