12/6/2016 6:08 PM | |
Joined: 8/8/2014 Last visit: 6/14/2022 Posts: 52 Rating: (3) |
Hi, I also met this error of -88 while trying wether to download or upload the project into the CPU. I tried diffrerent versions of my project. I program the PLC remotely (via VPN connection), so I'd like to keep network settings and hardware config and update only software remotely. Is it possible w/o factory reset, what MRES button in online panel will do ? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/7/2016 1:40:22 PMNew subject after splitting |
|
Follow us on