11/3/2021 5:25 AM | |
Joined: 11/2/2021 Last visit: 5/10/2022 Posts: 2 Rating:
|
Hello everybody, I'm using IOT2040 My base image is V3.1.1 when I run iot200setup->Peripherals-> "Show I/O Configurations" I also get an errror /sys/class/gpio/gpio45/value "Enable I2C on Pins A4 & A5" I also get an errror ValueError: Invalid i2c bus "Enable SPI on pins D1o-D13" I also get an errror ValueError: Error initialising SPI bus "Enable UART0 on Pins D0 & D1" I also get an errror ValueError: Error initialising UART Thanks please help me Kind regards Attachmenterror.pdf (365 Downloads) |
Follow us on