9/6/2016 2:04 PM | |
Posts: 111 Rating: (15) |
Hello ronaldo7, did you have access to the folder where the pdf-docs shall be saved? There is a error description in the SIMATIC chapter 14.1.2.12 which could be a reason for your error message: SIMATIC Process Control System PCS 7 SIMATIC BATCH V8.2 Perhaps there is no access to the described templates or the access is denied. Hope this can help you. |
9/7/2016 4:30 AM | |
Joined: 7/19/2013 Last visit: 5/15/2024 Posts: 68 Rating: (3) |
Hello, Yes I have access to the folder, because I can generate XML to that folder. I didn't delete the report template also.But I can't find file "standard_xxx_x.rdl" in my folder \SIEMENS\BATCH\RSTemplates. I attach the screenshot of my project setting and error message, hopefully you can help.
AttachmentBatchArchiveProblem.zip (111 Downloads) |
9/7/2016 9:45 AM | |
Posts: 111 Rating: (15) |
Hello ronaldo7, I think the reason of your error is that there are no templates in the folder for the PDF-creation of the report. If there are no templates, perhaps a reinstallation of SIMATIC BATCH can help or a manual copy of the templates in the folder "C:\Programs(x86)\SIEMENS\BATCH\Template" If there are some other template (not "standard"), try another template to verified that the process generally is applicable. You can also create your own report template, for that there are some application samples and FAQ, which show a way to create an own report template: How do you create and use a user-defined BATCH Report Template in PCS 7 SIMATIC BATCH? Configuring of SIMATIC BATCH Reports using a practical example How do you change a user-defined BATCH Report Template in PCS 7 SIMATIC BATCH? Hopefully this will help you. |
This contribution was helpful to1 thankful Users |
10/24/2016 4:47 AM | |
Joined: 7/19/2013 Last visit: 5/15/2024 Posts: 68 Rating: (3) |
Hello,
Do you think what other else the problem is? Thank you AttachmentBatchArchiveProblem.zip (81 Downloads) |
10/25/2016 1:27 PM | |
Posts: 111 Rating: (15) |
Hello ronaldo7, I'm sorry but I don't have a glue what's the error. I think the best way is to contact the technical support. I'm sure they can help you: via "Support Request" on the homepage: https://support.industry.siemens.com/my/ww/de/requests/#createRequest |
Follow us on