10/6/2015 10:25 AM | |
Posts: 1 Rating: (0) |
Dear Sirs, Please Help Error when Compiling Configuration of PLC S7-1200 on TIAportal V13 SP1. + Error indicator: Differences between configured and target modules ( online) , No action + Error indicator: Reset modules , No action Below message is with error : The compilation of the hardware configuration failed (C007 -60 -1998520320 2402).,,,3:10:09 PM When I Stop CPU, it displays message " The configured CPU and the CPU available online are different. Do you really want to put this CPU in the STOP mode?" Pls give me a hand for above errors. Thanks/ best regards I'm looking forward to hearing from you soon ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/6/2015 11:25:31 AMNew subject after splitting |
|
Follow us on