8/1/2016 3:28 PM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating:
|
Hello All, I am using PCS7 410-5H system in my configuration along with ET 200M IO modules. I am facing the problem with the system that i am not able to open the hardware configuration on my system. Whenever i tried to open the hardware configuration it is giving the error message "S7 hardware configuration has stopped working". On the other if i tried to open the hardware configuration through the Net pro then it is opened and if check for consistancy then also no error message shown. Please suggest that what could be the issue. earlier this error was only in one project, but now i am not able to open the hardware configuration for the new project as well. I have attached the screen shot for your reference. Best regards, Naresh Saini ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/2/2016 7:31:37 AMNew subject after splitting |
|
8/2/2016 8:45 AM | |
Posts: 567 Rating:
|
Hi nkr, does this problem occurs only on your ES with this project or also on other? Did you install or change anything on your system before this problem occurs? Maybe you have to make a new installation of your ES. The other possibility you have to contact the siemens technical support. They can analyze the diagnostic data (e. g. dump files) and give you a solution to solve this problem. You can contact the technical support over this link: Support Request |
8/2/2016 2:12 PM | |
Joined: 10/26/2011 Last visit: 7/17/2024 Posts: 762 Rating:
|
I read, that you have reinstalled your Engineering System and the problem exists furthermore. You can dearchive an older project status and test it with this. If everything is ok, it is possible, that your current project status has an defect. In case of defect, please contact the technical support, like Ralfino has posted. The technical support can try to repair the project. |
SIMATIC PCS 7 - Overview |
|
Follow us on