10/11/2013 12:23 PM | |
Posts: 8 Rating: (0) |
Thank you for answering me. But what I want to say is why when I download to the PLC, It errors as in the attached file. |
10/15/2013 10:35 AM | |
Posts: 8 Rating: (0) |
Dear Sir Please help me to check why when I use the address ET200M of the I/O Analog to error? You can see in Network 3 and Network 4 in OB35. Thanks! AttachmentET200M-Analog IO.zip (108 Downloads) |
Last edited by: Vudv at: 10/15/2013 10:38 AM |
|
10/15/2013 12:11 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello again, There is no problem if:
The problem may come from combination of PROFINET IO plus analog modules both in range of process image and even peripheral addresses.This is a problem that the software developers should answer it.Please try it here (Support Request). Best regards, Hamid Hosseini |
Follow us on