6/13/2018 9:52 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
Did you compile your project in TIA V13 SP2 after you installed the latest SP? |
FCK WAR! |
|
6/14/2018 3:19 PM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
Nope :) I will make this and I come back with a feedback |
6/14/2018 3:31 PM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
I compile the PLC. I attach a picture with the result. |
6/14/2018 3:32 PM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
I compile the HMI. I attach a picture with the result. |
6/14/2018 3:37 PM | |
Joined: 3/8/2016 Last visit: 7/4/2024 Posts: 13 Rating: (0) |
After I made the compile I save the project and I try to open with TIA Portal V14. I attach the error log. The update stops at 75%. It's a possibility to open this project in version 14 or I need to make the project in version 14 starting from zero? Thank you. AttachmentConversionLog_13.0.1.0_to_14.0.0.0[8].docx (266 Downloads) |
Follow us on