10/14/2022 11:38 AM | |
Joined: 8/6/2018 Last visit: 6/6/2024 Posts: 251 Rating: (39) |
Hello, Have you tried saving the project with slow reorganization? file>>save as>> With reorganization (slow) thanks you |
10/18/2022 12:22 PM | |
Joined: 3/11/2019 Last visit: 6/7/2024 Posts: 1460 Rating: (263) |
Hi, if no message to missing software packages are shown, this should not be an issue for the crash. But as i can see on the screenshot, a very old version is used (STEP 7 V5.6 + hotfix 1). In the meantime STEP 7 V5.6/Professional 2017 with servicepack 2 + hotfix 9 is available. At first i would recommend an update to the current version (no other license needed). regards sancruz STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial DownloadDownload Hotfix 9 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2 |
Feedback appreciated, please rate |
|
Follow us on