9/3/2010 2:59 PM | |
Joined: 8/18/2010 Last visit: 3/18/2023 Posts: 42 Rating: (9) |
Thank you for the suggestions, Huggy_d1. I will give that a try. |
9/3/2010 3:01 PM | |
Joined: 8/18/2010 Last visit: 3/18/2023 Posts: 42 Rating: (9) |
Pegaia, what files do I need to upload? Is it only the .ap10 file? |
9/3/2010 10:20 PM | |
Joined: 9/23/2005 Last visit: 10/4/2024 Posts: 4349 Rating: (1446)
|
Hi, you need to send all data (in a zip archiev). |
Denilson Pegaia |
|
9/3/2010 11:34 PM | |
Joined: 8/18/2010 Last visit: 3/18/2023 Posts: 42 Rating: (9) |
Here is the ZIP file of the Project folder.
AttachmentProject1.zip (404 Downloads) |
9/4/2010 3:54 AM | |
Joined: 10/7/2005 Last visit: 10/6/2024 Posts: 3024 Rating: (1054) |
Hello Saint Germain I can see three issues in your program which cause the compile errros: 1.) FB3 NW1 has open branches (see yellow highlight in attached screendump) 2.) FB1 NW4 has missing addresses (see greenhighlight in attached screendump) 3.) DB 2 exists twice in your program (once declared as Modbus Master DB and once declared as Modbus Slave DB, seeredhighlight in attached screendump). Number 1 & 2 are easily fixed. As for number 3 I'mnot too sure how you managed to end up with two DB's with the same number in your program but suggest you simply change one of them to a different number. I hope this helps |
Cheers |
|
Follow us on