3/1/2020 9:25 PM | |
Posts: 3 Rating:
|
Hello, I am attempting to install SIMOTION Scout Ver 4.4 HF 11 which I got from this page. The laptop is running 64-Bit Windows 7, SP1 with a 8GB Intel i7 processor During installation I get told to the log file for the installation errors. The error(s) are in the attached pictures. You can acknowledge the error but it keep popping up. Additionally, it is stuck on the "Installing DCC DCBLIB SIMOTION". The progress bar actively fills but then starts over once it hits the end. If you cancel, it just aborts the entire installation. I was wondering if anyone may know of a work around. A thought I had is that I was missing some sort of update file, or something to that effect |
Last edited by: Jen_Moderator at: 03/02/2020 12:21:36Optimized link. |
|
Follow us on