2/5/2013 5:10 PM | |
Joined: 2/5/2013 Last visit: 3/26/2024 Posts: 287 Rating: (5) |
Thanks for the fast reply! Silent Bob: I've executed the Right program on the shared destination forder on OS1, but got the same result, should I run it also on OS2? RugbyGuy: Win7 is Ultimate the name of PC seems to be the same, but sometimes when you access OS1 from network it appear as os1 also if on the PC properties is upper case. I'll look at the link you've sended and let you know. Thanks! |
2/6/2013 8:10 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Hello Summer88, Have a look on the Post by Bilal Moolla Downlaod the File & follow the Step given in the file...... May be have a look on this will Help you tpo solve the Problem..... |
Ammy |
|
2/6/2013 4:46 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
Same image as in using the rebuild A1 or A2 disc? Or did you build up the PC with a name (example ES1) image it, then reload onto the server (change name to OS2)? If it is the second one, then this could very well be the issue. PC Names can only be named 1x. There are places in SQL and WinCC that do not take very well to a PC name change. Please see this link for detailshttp://support.automation.siemens.com/WW/view/en/5708281 I recommend rebuilding the PC with the name change from the beginning.
|
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
Follow us on