3/21/2018 9:58 AM | |
Posts: 3 Rating: (0) |
Hi All. Need some assistance with connecting an HMI. I have a ET 200SP CPU with a bus adaptor and want to connect to an INVT HMI through Profinet. The HMI gives me an option to select an link SERVER AG as Device and a SIMATIC S7 as Server. Can this be doen and how does it work? How do I set up the CPU to recognize the HMI. I'm playing around in the dark at the moment as I have never done this before, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/21/2018 1:13:22 PMNew subject after splitting |
|