12/24/2019 12:09 PM | |
Joined: 12/27/2018 Last visit: 7/19/2024 Posts: 510 Rating: (43) |
Hi Friends I need an urgent help. I am trying to commissioning a project with Siemens S7 1500 PLC( 6ES7 515-2AM01-0AB0 ;Firmware V 2.6) and ET200MP( 6ES7 155-5AA00-0AC0; Firmware V4.2),DI 32x24VDC HF Firmware-V2.0-1No, DQ 32x24VDC/0.5A ST_Firmware-V2.0-1Nos; AI 8xU/I/RTD/TC ST_Firmware-V2.0-8Nos. Software- TIA Portal V15.1 Upd 3 Laptop-PG M5 Program compiled and no errors Problem: 1.CPU -RUN(Green) and SF(Red) Blinking 2. ET200MP - Green LED of all IO modules connected to ET200 Module blinking 3.Red color shaded circle next to CPU in project tree while online 4.Disconnect simbol on ET200MP online device view Diagnostic: IO device failure-IO device not found (This ERROR still persisting) Diagnostic report and :Attached I have checked previous post on the same subject.ET200MP module dont have dark/light base module, Network topology is connected. Solution tried: 1.Ethernet cable connected both two port of CPU, Now port related issue solved from diagnostic 2.Removed all components and installed only one DI,DO,AI and a sample program made and downloaded. No changes on fault. Video attached. Please help me with solution. Attachmentdiagnostic report and pic.zip (98 Downloads) |
Last edited by: JKV JAMES at: 12/24/2019 16:25:54Jinson Kurian Vilayil James, P.Eng, BE, M.Tech (Power Electronics and Power System),PGDM, MBA |
|
12/25/2019 5:24 AM | |
Joined: 12/27/2018 Last visit: 7/19/2024 Posts: 510 Rating: (43) |
Thanks for your reply. The Green LEDS of the Signal modules are blinking.I will check it today at site and reply about 24V and sequence. I have upgraded firmware version of CPU and IM as per diag report earlier. I am not able to access the diagnostic to each signal modules such as shows disconnected symbol at online device config of all signal modules on ET200MP.Also sometimes not able to go online as well. Shall I need to add any gsdml file for ET200MP?I am using just ethernet communication. Is there any special configuration for this device? When I connect PLC and ET200MP in same PLC subnet, the ethernet indication LED turns from Green to Yellow, not blink? Any suspicious? Attachment: Online device config. shows disconnected sig modules. Why?Also red lines in Topology. Attachmentdevice config.zip (96 Downloads) |
Last edited by: JKV JAMES at: 12/25/2019 05:30:17Last edited by: Jen_Moderator at: 12/25/2019 13:00:02Optimized link. Last edited by: JKV JAMES at: 12/26/2019 16:12:50Jinson Kurian Vilayil James, P.Eng, BE, M.Tech (Power Electronics and Power System),PGDM, MBA |
|
Follow us on