Industry Online Support
Technical Forum
3/2/2014 7:16 PM | |
Posts: 4 Rating:
|
Hello, my name is Edgar and I am from Puebla México Please can you tell me, how did you solve your trouble? Currently I am working with 2 ET200PRO FC mountend in the SLOT 16 and 17 of an IM154-8 CPU. The IM154-8 is connected via PROFIBUS to other 15 IM154-8 PN/DP CPUs until a CPU319. I can download the HW config to the IM154-8 CPU and get green all the status LEDS, then I insert the STARTER Commissioning module to the FC module in SIMATIC manager VIEW When I open STARTER, I see the FC modules below the IM154-8 CPU but I can not reach them by the S7ONLINE or DEVICE interface by means of the RS232 optical interface. Then I go to the Project menu and with the option "Reachable Nodes" I can see and integrate them to the STARTER project and develop the commissioning!!. But they are out of the IM154-8 CPU project so I can not reach them by the user program!! What is wrong? Greetings
AttachmentET200_PRO_HW_Config.zip (221 Downloads) |
Follow us on