9/2/2014 1:54 PM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Greeting, We wish to measure the frequency and counting with the help of 6ES7138-4DA04-0AB0 module, using FREQUNC_300C function block we have attached parameters but didn't receive any information on DB2.DBD14 and DB2.DBD18...?? also please guide for the wiring connection we have pulse generator with 24vdc output which one terminal we can use for clock pulse should we use only terminal 5..?? Can we use 6ES7138-4DA04--0AB0 with 6ES7151-1CA00-3BL0..?? Thanks. AttachmentDesktop.zip (686 Downloads) |
Last edited by: Sarfraz Bhatti at: 9/3/2014 10:36 AMMS |
|
9/12/2014 9:18 AM | |
Joined: 4/24/2006 Last visit: 8/14/2024 Posts: 8714 Rating: (1166)
|
Hello, Here is a link to manual: SIMATIC ET 200S Technological Functions Please have a look at page 75 The measured value will be accessible by First 4 input bytes. Best regards, Wizard |
9/12/2014 12:02 PM | |
Joined: 4/24/2006 Last visit: 8/14/2024 Posts: 8714 Rating: (1166)
|
Hello, Perhaps the following link might help: With the ET 200S electronic modules 1 COUNT 5V/24V, how do you save and retain the counter value or start counting again from the old counter value after a restart? Best regards, Wizard |
3/17/2017 2:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by DavidMolina is split to a separate thread with the subject Configure counter 24v/100khz with IM151-7 in TIA Best regards |
Last edited by: Min_Moderator at: 3/17/2017 2:22:19 PM |
|
Follow us on