8/16/2016 11:33 AM | |
Joined: 11/29/2013 Last visit: 5/21/2024 Posts: 98 Rating:
|
I'm considering using the ET200SP for a new project, but this is a rather particular case and I will need the controller to act both as Master and Slave DP device. The 6ES7545-5DA00-0AB0 module can be configured act as both, so I assumed I could add two of these and configure one as master and the other as slave (I do this in the S7-1200 using in CP1243 and one CP1242). However, while configuring the hardware in TIA portal, it appears that I can add only one communication interface to the CPU. Is there any way around this? Thanks! Rodrigo |
8/16/2016 11:46 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Rodrigo, this shoud depend on the CPU. but in technical data of the 6ES7512-1DK01-0AB0 is only one PB-interface mentioned regards, |
FCK WAR! |
|
Follow us on