3/5/2020 8:07 PM | |
Joined: 9/21/2012 Last visit: 8/12/2024 Posts: 4087 Rating: (459) |
You can use the modules own QBAD bit. |
3/6/2020 5:05 PM | |
Joined: 9/21/2012 Last visit: 8/12/2024 Posts: 4087 Rating: (459) |
What program are you using? TIA or Simatic Manager? |
This contribution was helpful to1 thankful Users |
3/6/2020 6:10 PM | |
Joined: 4/28/2015 Last visit: 8/6/2024 Posts: 25 Rating: (0) |
I am using Simatic Manager v5.6 |
3/11/2020 10:28 AM | |
Joined: 4/28/2015 Last visit: 8/6/2024 Posts: 25 Rating: (0) |
Anyone have idea about this ...sent from App |
3/11/2020 10:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi, there are FAQ and application samples for this: With diagnostics-compatible modules how do you evaluate a change of the diagnostics status in the user program of the S7-300?PROFINET IO – Diagnostics Processing in the User ProgramThese entries are findable with the search bar in the upper right. hope this helps, regards, |
FCK WAR! |
|
7/23/2020 2:45 AM | |
Joined: 4/18/2016 Last visit: 7/30/2024 Posts: 19 Rating: (2) |
The "GET_DIAG" instruction is used to read the diagnostic information of a hardware component. |
Follow us on