8/7/2023 12:21 AM | |
Joined: 7/17/2023 Last visit: 5/9/2024 Posts: 10 Rating: (0) |
Hi Guys, I ran into an issue: HW config and Chart can be downloaded successfully, left CPU is Master and right CPU is Slave and both are in Run. But the remote I/O racks are not recongnized. it is shown Module configured, but not available. The remote IM-155-6 module information is attached. what could be the cause? Thanks in advance. My sysytem information as below: 1. PCS 7 V8.2 SP1 system; 2. Redundant CPU rack, 6GK5208-0GA00-2FC2 (SIMATIC PCS 7 CPU 410 REDUNDNCY, 2x CPU, 2X SYSTEM EXP. CARDS, 2X2 10M SYNC MOD., 2 CP443); 4. Three I/O chassis (IM155-6 v1.2); 5. Windows 10. AttachmentBoth CPU in Run.zip (279 Downloads) |
Last edited by: Shijun07 at: 08/07/2023 00:23:55 |
|
8/10/2023 6:24 PM | |
Joined: 7/17/2023 Last visit: 5/9/2024 Posts: 10 Rating: (0) |
Hi, Taru, First, we are missing the CPU 410 Expansion RACK (PN Red) license. Now I have followed section 2.6.4 to get the license for CPU in Rack 0 upgraded. But I cannot find the folder mentioned in the manual 2.6.4. Do you know where the activation file is located? In my ES, there are three users, the real user is gasco, the computer name. the others are default and public. In any of the users, I cannot find the folder mentioned in the manual: "Documents > Siemens > Automation > PCS 7 > Activations" I attached the manual and screen captures. Please help. Thanks. AttachmentFiles.zip (200 Downloads) |
Last edited by: Shijun07 at: 08/10/2023 18:25:58Last edited by: Shijun07 at: 08/10/2023 18:26:15Last edited by: Shijun07 at: 08/10/2023 18:27:49Last edited by: Jen_Moderator at: 08/11/2023 09:24:46All files added as .zip file. |
|
8/15/2023 8:03 AM | |
Joined: 1/11/2019 Last visit: 5/22/2024 Posts: 702 Rating: (140)
|
Hello,
|
Follow us on