11/14/2016 10:58 AM | |
Joined: 6/29/2012 Last visit: 12/25/2023 Posts: 975 Rating: (7) |
Is the lean Ethernet card : 6GK7 343-1CX10-0XE0 compatible with the plc : S7 315 : 6ES7 315-1AF03-0AB0? |
11/14/2016 12:30 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, Go to table 2-1 B-9 should work: S7-CPs for Industrial Ethernet - CP 343-1 Lean (CX10) - Siemens (as of hardware version 2 and firmware version V2.2) |
Last edited by: Ste39 at: 11/14/2016 12:32:16 PM |
|
11/14/2016 12:31 PM | |
Joined: 7/9/2015 Last visit: 4/26/2024 Posts: 3814 Rating: (554) |
Hi, yes it´s compatible: Check PN CP 343-1 Lean Manual Part B. In chapter 3 you can check PLC which can be used with you CP - There you can also find your CPU 315. Regards, Towome |
|
|
Follow us on