6/5/2019 6:42 PM | |
Posts: 59 Rating:
|
Hi, My laptop installed with TIA V13 and logo soft comfort v8.0 is not sensing ethernet port after installation of Schneider SFT2841. Is the SFT2841 installation the reason or are there may be other reasons for not sensing ethernet port when a device is connected to the ethernet port. Proneta is also showing no adapter selected and laptop actual adaptor selection field is not selectable. Can anybody advise solution? ------------------------------------------------------------------------------------------ |
Last edited by: fiah at: 06/05/2019 18:46:36Last edited by: Jen_Moderator at: 06/06/2019 10:42:22New subject after splitting |
|
12/23/2020 2:41 PM | |
Joined: 9/16/2019 Last visit: 8/21/2023 Posts: 12 Rating:
|
USB ethernet adapter is working perfectly. |
Follow us on