12/28/2017 3:14 PM | |
Posts: 23 Rating: (0) |
this my network adapter screen shoot |
12/28/2017 3:30 PM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33780 Rating: (4194)
|
Maybe that the not correct installed PCI Simple Communications Controller the problem is? |
12/28/2017 3:50 PM | |
Posts: 23 Rating: (0) |
I have update...but still..problem Thanks |
12/28/2017 4:12 PM | |
Posts: 23 Rating: (0) |
MY Aplication.ini diffrent.. the " PORT = com 1 " do you have solution ? Thanks |
12/29/2017 9:07 AM | |
Posts: 23 Rating: (0) |
Hello Maybe , i get the problem..its cause hardwere driver not suitable with LSC Because I have install this LSC v8 Softwere to another computer , Its sucsess to identify wireless LAN But for Ethernet is same ..NO HIGHLIGHT ..cause the driver same with my current computer. Maybe tonight .. i will buy USB to Ethernet .. I hope this problem can be solved I'm Attach the last screenshot Thanks AttachmentLan.pdf (129 Downloads) |
Follow us on