3/30/2022 7:23 AM | |
Joined: 5/27/2014 Last visit: 10/26/2022 Posts: 109 Rating: (6) |
Hi, I'm trying to establish communication between EthernetIP device (Allen Bradley Power monitor 500 1420-V2-ENT 5.002) and Siemens 1516f plc. I followed this guide EtherNet/IP Scanner – Connecting third party I/O’s using EtherNet/IP. It's kind of confusing to get Assembly instance, Packet interval, Input/output size/identifier from eds file, but I believe I got it correct. When I run the code, status of LCCF_EnetScanner FB is 7002 (Follow Up call), but no data is being exchanged. When I capture traffic, I can see packets are being exchanged, but Connection manager is failing. Any ideas? Thanks
Attachment0001009200070500.eds.zip (409 Downloads) |
TIA V16 update 4, STEP 7 Professional+safety |
|
3/30/2022 8:40 AM | |
Joined: 8/31/2013 Last visit: 4/18/2024 Posts: 606 Rating: (41) |
Hello, Does your Scanner supporting Modbus Communication via Ethernet IP ? |
Warm Regards |
|
Follow us on