4/4/2023 5:59 PM | |
Joined: 6/1/2022 Last visit: 4/26/2024 Posts: 23 Rating: (0) |
I`m following this tutorial to Evaluation of the PLC Status "RUN/STOP": https://cache.industry.siemens.com/dl/files/628/109481628/att_963562/v2/109481628_PLC_Status_WinCC_TIA_DOC_en.pdf But it`s not displaying the status on HIM in the symbolic IO field that I made. I followed all the steps according this tutorial. Attachment109481628_PLC_Status_WinCC_TIA_DOC_en.pdf (229 Downloads) |
Last edited by: Jen_Moderator at: 04/05/2023 07:54:21PDF attached from link. |
|
4/4/2023 6:39 PM | |
Joined: 6/1/2022 Last visit: 4/26/2024 Posts: 23 Rating: (0) |
I'm trying with two differents PLCs an S7-1200 1214C and an 1215C. |
4/4/2023 7:01 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066) |
Then make you something wrong. Please can you upload your TIA project? |
4/4/2023 7:37 PM | |
Joined: 6/1/2022 Last visit: 4/26/2024 Posts: 23 Rating: (0) |
Here is the part that I'm having this problem.
AttachmentForun.zip (106 Downloads) |
4/4/2023 7:41 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066) |
I'm sorry, but I don't have TIA V17. |
4/5/2023 11:18 AM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066) |
Do you know this FAQ from Siemens? How do you evaluate the "RUN / STOP" mode of the CPU via an HMI operator panel?There is a example for TIA V15 that you can download. |
Follow us on