10/22/2012 7:45 PM | |
Posts: 3 Rating:
|
I have a problem with a CPU315 2DP. The next error message appears on diagnostic buffer and the cpu dont RUN. Regardless the configuration tested, these two event appears again and again... I am totally desapointed and desperate See attached file for more explanation. Event1 of 128: Event ID 16# 49A0 STOP caused by parameter assignment error or unpermissible difference between preset and actual configuration: startup disabled No relevance for user (SDB no.): 1 No relevance for user (Z2): 0250 (Z3): 8805 Previous operating mode: STARTUP (warm restart) Requested operating mode: STOP (internal) External error, Incoming event 02:46:29.974 PM 10/18/2012_____________________________________________________________ Event 20 of 128: Event ID 16# 5962 Parameter assignment error preventing startup in CPU module parameters Parameter: area Output address: 592 of the module with parameter assignment errors Error type: parameter not in permitted range Operating mode: STOP (internal) External error, Incoming event 02:46:24.415 PM 10/18/2012 (This is not output 592 in my config!!) AttachmentConfig.zip (413 Downloads) |
Last edited by: Raph_GY at: 10/22/2012 7:48 PM |
|
10/22/2012 10:24 PM | |
Joined: 9/27/2006 Last visit: 8/6/2024 Posts: 12273 Rating:
|
Hello Raph; |
This contribution was helpful to
1 thankful Users |
1/19/2021 6:06 AM | |
Joined: 7/7/2018 Last visit: 7/21/2024 Posts: 11 Rating:
|
Hello sir, I have same issue but little different, we have Schneider drive slave and slave Remote profibus DP IO. We are facing some issue that Remote panel (Slave 8)getting stopped, it is the last device in the network. Before this we have Schneider drive (Slave 7). it was stopped and started. Now running but sometimes making this issues. we already changed profibus connector. In simatic manager we already installed OB82, OB86. Is there is any problem in cable? how i can rectify this issue.
|
Follow us on