2/12/2016 12:08 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Hello, The .EventState is a PCS7 structure tag included in technology blocks which have a message system (MsgEvId). .EventState ensures that all blocks have the same structure to display statusses. Each bit in the 32-bit word has particular significance and changes depending on incoming/outgoing events. The .EventState is generated automatically, so changing the values of the tag is not recommended. Additional info: When using chronological messaging, the data for the group display are made available in the "*.EventState" tag. You can link the "Group Value" property of the group display directly to the "*.EventState" tag. Entry ID 23730649 and Entry ID 23730697 provide detailed information on chronological messaging and the associated requirements. When using the bit alarm procedure or the analog alarms, the "*.EventState" tag is not available by default to provide the group display with the message status. |
Last edited by: Oreca at: 2/12/2016 12:27:49 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/12/2016 4:39 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Here you go! (enclosed) AttachmentEventState.pdf (1078 Downloads) |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/12/2016 5:23 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
You forgot the screenshot |
If I could help you, you can use the RATE button. Thank you. |
|
2/15/2016 5:05 PM | |
Posts: 72 Rating: (2) |
It is in my first post Thanks for your help |
2/16/2016 2:58 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Hello, Oh, I thought you meant that you had another document enclosed. I assume it's a test project...Did you activate Alarm logging? Did you run OS project editor? The group display will take message classes/types from PCS7 alarm logging by default setting. If they are not defined, maybe there lies the problem. Overall, numerous things can be wrong. Did you did a OS compile, download etc.. to make sure all settings are transferred, so basically everything is at default setting? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on