11/9/2011 8:44 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Hoping to please, I enclose an example of communication between Modbus TCP s7 1200 (master) and Zelio Logic (slave). I used a Zelio as a slave because it was the only device that modbus tcp aho available at this time. Joseph AttachmentTest Zelio modbus TCP (software per S7 1200).zip (1679 Downloads) |
Last edited by: automatizzando at: 4/3/2012 10:17 PM |
|
11/9/2011 8:47 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
I attach also the software to be loaded in the Zelio
Attachmentsoftware per zelio (slave).zip (763 Downloads) |
Last edited by: automatizzando at: 4/3/2012 10:10 PM |
|
3/14/2012 10:00 PM | |
Posts: 1 Rating: (0) |
Your zip file for the Zelio is empty .... No application there! |
4/3/2012 3:53 PM | |
Joined: 11/15/2007 Last visit: 3/23/2024 Posts: 11 Rating: (2) |
That's true - nothing inside..
|
4/3/2012 10:11 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Now it should work. Hello and thanks |
7/18/2013 10:38 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Follow-up-question splitted to slave is RS422 and two master is RS485 Best regards O_Moderator |
7/25/2013 1:05 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was splitted to MB_MASTER, Configuration datails Best regards O_Moderator |
Follow us on