8/31/2012 5:50 AM | |
Posts: 7 Rating: (0) |
Hello Jon Thanks for your reply !! The slave in question isDIGUREG (RG3-DUR)system from Siemens. The exchange of the signal is done with this DIGUREG system. The profibus siganl exchange listwith the DIGUREG system is attached herewith. Regards Vashist AttachmentE:\PKV_Folder\Projects\01_Standard\02_Standard_RG3-DUR\Profibus Signals\ProfibusDIGUREG_e.pdf (190 Downloads) |
8/31/2012 6:55 AM | |
Joined: 10/7/2005 Last visit: 9/18/2024 Posts: 3021 Rating: (1054)
|
Hello Vashist I am speculating here, but my guess is that the DIGUREG uses Little Endian format. If this is the case and sinceSiemensPLC's use BigEndian format, the high and low byte of each word (e.g.Integer value) need to be swapped, hence the CAW command. I hope this helps and you'll find more info about the Little vs Big endiandifferences at http://en.wikipedia.org/wiki/Endianness |
Cheers |
|
Follow us on