5/22/2012 4:34 PM | |
Posts: 621 Rating:
|
Hi all is there possble to expznd the meomory in cross referance area..and how..? regards algudkar |
5/22/2012 6:20 PM | |
Joined: 1/3/2006 Last visit: 7/26/2023 Posts: 726 Rating:
|
Hi, Expand the memory in cross reference area. What the hell does it means on this good Earth ?? |
5/22/2012 9:47 PM | |
Posts: 621 Rating:
|
Hi IBN-Service thank you very much i got your point. just for my knowledge purpose iam askinking this here i attached 4 photo snap plz check it. in M1 snap that is previous project referance data.in the second snap what iam calling the address bit byte,word MB QB IB etc that is updating in the referance data table ok.in the third snap once i created the network and asigned the adress MB,QB IB's it will update in referance data table. you clearly mentioned that above automatically last used adress. NO need to adjust manually. so my question is.there depends on memorycard or plc memory. whynot to take the byte or bit memory before creating the programm. so wht is the limitation was red DB,FB,FC are having thae limitation 0 to 65, 365numbers but not sure.so here is also any limitation or restriction.. its for my knowledge..purpose. regards algudkar Attachmentmemory.zip (23 Downloads) |
Follow us on