10/10/2018 4:41 PM | |
Posts: 4 Rating:
|
Bonjour, je cherche à raccorder un automate siemens S7-300 à un système EXPERION Honeywell via un coupleur CP343-1. nous avons mis un CPU S7-300 avec firmware V3.2 et le système EXPERION SCADA ne voit pas l'automate. nous arrivons à pinguer le SCADA. est ce que quelqu'un a une solution?? merci d'avance.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/11/2018 10:02:18 AMNew subject after splitting Last edited by: The Helping Hand at: 10/11/2018 10:03:25 AMAdded english translation via Google Translator. Last edited by: The Helping Hand at: 10/11/2018 10:04:49 AM |
|
10/11/2018 12:06 PM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating:
|
Hi, do you use the Modbus blocks? Wüstenräuber |
10/12/2018 9:47 AM | |
Posts: 4 Rating:
|
Hi, yes we use the Modbus blocks and the connection online state is ok. Cordialement. |
10/12/2018 12:18 PM | |
Posts: 3093 Rating:
|
Hello; Which error does MODBUSPN report? Regards, |
10/12/2018 5:23 PM | |
Posts: 3093 Rating:
|
Hello, Regards, |
10/16/2018 8:36 AM | |
Posts: 3093 Rating:
|
Just to complete Duris' post: client is the active communication partner, it sends requests. Server is the passive one, it responds. |
Follow us on