3/4/2007 6:09 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, I have looked on the page but there is only information about the functions, not about the programming. Are there possibilitys to work with the engineering packages, or is it like S7 Lite, only to use for small PLCs and without any networking, drives and all special cards. If it is only for the DBs then I could earn easally the money by doing it with the tool that Siemens have by there own. How do you import an Excel list with STEP 7 variables into a data block? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
4/28/2007 3:30 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Please look for the next link: STEP 7 InfoBrowser V1.0 - Exporting STEP 7 project data to MS-Excel and accessing information in Online Support This will help you to the right way I think. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to1 thankful Users |
2/20/2008 10:57 AM | |
Posts: 2 Rating: (0) |
Oh ! thanks. |
5/2/2011 1:02 PM | |
Posts: 30 Rating: (0) |
-------------------------------------------------------------------- Hi the page www.s7xp.com not found. Please give me the right address |
Last edited by: eemi at: 5/2/2011 1:03 PM |
|
5/26/2011 9:31 AM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
I'm interested too, I tried the STEP 7 InfoBrowser tool but it fails to load the full project, displaying an error, see attached screenshot. Copy/paste is also not good cause it doesn't include the address column Opened an older project with STEP 7 InfoBrowser and it works, so probably the newer project uses resources that STEP 7 InfoBrowser doesn't know. |
Last edited by: SteBo at: 5/26/2011 9:39 AMB r g d s , |
|
Follow us on