9/15/2016 12:45 PM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating:
|
Hi, Make sure you select the project inside the multiproject. The demo multiproject is called "color_gs_MP" and you must select "color_gs_prj". Then select Edit->Export. The name: "Export as XML" does not exist, so the manual is wrong. When the dialog is shown, the file format is set to .XML automatically. If you still don't see it, it means you probably don't have PCS7 installed but only Step 7. You can check the installed software under Start->Siemens Automation->SIMATIC: "Inst. software".
|
Last edited by: Oreca at: 9/15/2016 12:47:47 PMIf I could help you, you can use the RATE button. Thank you. |
|
9/16/2016 11:14 AM | |
Posts: 567 Rating:
|
Hi, you need the software component SIMATIC XML-Transfer. This should be installed with SIMIT V8.1. |
This contribution was helpful to
1 thankful Users |
9/16/2016 11:19 AM | |
Joined: 3/14/2008 Last visit: 7/11/2024 Posts: 2075 Rating:
|
Hmm, Your color_gs_prj is removed from the multiproject for editing, your MP project indicates this by the icon which is transparant. Maybe the export function does not work then. Can you retrieve a backup of the example project? And check if it works when the color_gs_prj is inside the MP project? @Ralfinio: I have PCS7 v8.2 installed, no SIMIT, but the export option is available to me. |
If I could help you, you can use the RATE button. Thank you. |
|
9/23/2016 3:01 PM | |
Posts: 8 Rating:
|
All the information regarding the tutorial can be found here. Whenever I start the manager I get the following notification. Could this be the source of my problem? |
8/24/2018 3:12 PM | |
Joined: 6/8/2016 Last visit: 6/27/2024 Posts: 6 Rating:
|
Hello AutoGen, did you resolve the problem? Greetings, Damian |
Follow us on