12/10/2014 2:31 PM | |
Posts: 11 Rating: (0) |
Hello, I'm having issues with a DP-Slave (Matrix Sign from BRIMOS with the correct GSD) which is causing an 'external fault' (The Matrix Sign itself functions properly even with the fault). The help event refers to the cable or connector not being well connected, But these are both pre-fab cables/connectors from the supplier. The supplier says that the fault may have to be reset within the Siemens Hardware configuration, but doesn't know how (They don't use Siemens....). In the diagnostics there is call to OB86 which cant be loaded. Not sure if this is causing the issue. OB86 is added in the online block folder. I've tried different OB's and disable interrupts SFC's but made no difference. I've added some attachments of the issue. Help/tips on the issue would be much appreciated! Thanks Danny AttachmentMSI test.zip (66 Downloads) |
Follow us on