2/15/2024 8:22 PM | |
Joined: 1/4/2024 Last visit: 10/10/2024 Posts: 5 Rating: (0) |
Hello siemens enthousiasts. New day new struggles. I`m working on a 840d SL 4.5 with i believe pcu50 The trouble i am having is getting the extopen command to work. In the past i have created a network connection between Windows Pc and the milling machine. Sharing folders is not a problem, i can copy, paste and see the files on both systems. i`ve read : - https://support.industry.siemens.com/cs/attachments/109477198/109477198-Application_Integration_of_SINUMERIK_840D_sl_in_company_network_en.pdf multiple times. aswell as a bunch of other manuals. All the other manuals refer to a extdev.ini file This file is not present on my machine. The folder structure cf-card or user does not exist at all. Nevertheless the other manual got me hooked up with a solid network connection. Which functions fine with copy and paste. this pic. shows an example on drive 2.This is the exact way i have created my share/connection on drive 4. but my extopen doesn`t work. it always returns a value of 2.(or 16 when i made a typo) (2 == External device is not configured) (16 == Invalid external path has been programmed) --------------------------------------------- DEF STRING[100] PATH="/DEV/EXT/4" DEF INT ERROR_OPEN EXTOPEN(ERROR_OPEN, PATH, "SYN", "SHARED", "APP") IF ERROR_OPEN > 0 MSG("Error for FILE OPEN ="<<ERROR_OPEN) M0 ENDIF STOPRE ----------------------------------------------- which is odd to me because copy and paste goes fine. the connection is there. I`m sure i am missing something but i cant seem to find it. Thanx for reading, hoping for help. Cheers. Attachment109477198-Application_Integration_of_SINUMERIK_840D_sl_in_company_network_en.pdf (261 Downloads) |
Last edited by: Jen_Moderator at: 03/22/2024 07:27:39PDF added from link. |
|
2/17/2024 5:37 PM | |
Joined: 6/30/2013 Last visit: 10/7/2024 Posts: 15 Rating: (1) |
Hi, You must configure "[ExternalDevices]" section in "extdev.ini". Refer attached template. Good Luck!!! Rgds, Chetan Attachmentextdev.ini.txt (305 Downloads) |
2/19/2024 6:15 AM | |
Joined: 1/4/2024 Last visit: 10/10/2024 Posts: 5 Rating: (0) |
Chetan_Verma,Thanks for your answer, As i mentioned in my post, the file does not exist on my machine. Neither does the folder structure. so i have no clue where to paste this extdev.ini file. Also curious why non of this in mentioned in: - Integration of SINUMERIK 840D sl in company network https://support.industry.siemens.com/cs/nl/en/view/109477198 cheers. |
Last edited by: The Helping Hand at: 02/19/2024 10:06:30Link optimized |
|
Follow us on