1/27/2009 9:35 PM | |
Posts: 26 Rating: (0) |
Is there a manual that contains the variable list and descriptions of F_GLOBDB? I am curious if there are others than .VKE0 and .VKE1 that may be useful. |
1/28/2009 5:36 AM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12294 Rating: (2691) |
Hello Swright; Here is an attachment containing adescription of the F-shared DB ("F_GLOBDB") of the safety program; it is extracted from the manual "Safety Engineering in Simatic S7": http://support.automation.siemens.com/WW/view/en/12490443 The document explains that the F-shared DB is generated everytime you compile a Safety program, to make your safety data available to your standard program blocks. So there is no generic table for this DB, the data it contains and the structure it is built on will vary depending on the F-blocks you are using in the F-program. Hope this helps, Daniel Chartier |
Follow us on