5/6/2013 8:04 AM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Hi, The simplest way to create a faceplate in WinCC is picture window creation. There is no need of any addional scripting required for the simple faceplate. Please find the linkfor the WinCC manual which contains detailed information about picture window. Revert back for clarifications. |
_______________________________________________________________ |
|
5/6/2013 8:39 AM | |
Joined: 1/28/2009 Last visit: 10/6/2024 Posts: 6852 Rating: (1365) |
Hello, I am sure there are already discussed threads in the forum with elaborated samples.The way you can access them is to SEARCH and read threads you are really interested in: create a faceplate with a single button which can set/reset a bit in an external tag Creating faceplates in WinCC V7.0, SP1 |
Follow us on