3/9/2022 9:11 AM | |
Joined: 2/8/2022 Last visit: 4/27/2022 Posts: 5 Rating:
|
Dear, I want to make a faceplate that goes up a value every time I push it. In the old HMI comforts I could just link an event to the symbol of my faceplate (a valve) to it "increase tag". The problem is that I would have to write a script myself now.So the intention is that every time I push on the faceplate the value is increased by 1. The value I want to increase is a tag interface (see attachment). This value is then linked to an HMI tag in the program and so on. Can anyone help me with this? Attachmentverhoog.zip (58 Downloads) |
3/9/2022 10:26 AM | |
Joined: 2/8/2022 Last visit: 4/27/2022 Posts: 5 Rating:
|
Thank you for your reply. But it doesn't work exactly yet. I don't have much experience with this but I have to make this in order for my internship. So I link the internal tag to an HMI tag. This in turn is connected to a PLC tag (DB). Furthermore, there is a small program for some things to control, but I do not think this is relevant. It's really just the intention that every time I push on the faceplate. This value is increased by 1. In the older versions this was all fairly simple but with the unified I can't get it done. afterwards I will then turn the cover of the faceplate gray at, for example, value 1 (position automatically), at value 2 for example green (handmatic) ,...
AttachmentJJ.zip (57 Downloads) |
Follow us on